This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWRL6432: Is it possible to use wakeup signal from two GPIOs at the same time?

Part Number: AWRL6432
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

Hi team,

When we select LPDS wake up source, we can choose only one pin from GPIO or SYNC_IN (like below in SysConfig).

If customer want to use two GPIO, Can they get the Wakeup signal from two GPIOs at the same time

And can we distinguish two GPIO sources?

*Customer will use two of the GPIO-WU_REQIN PINs at the same time.

Regards,

Lina