This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2114EVM: Not connected

Part Number: FDC2114EVM
Other Parts Discussed in Thread: FDC2114, LDC1101, FDC1004,

Tool/software:

I've installed the EVM GUI and driver and attached the USB cable to link my PC.

I can see the device in Device Manager listed as a USB Input Device (disappears if I disconnect the cable).

However, the GUI just shows 'Not Connected' in the lower left of the window.

I've tried on a Win10 PC and three different Win11 PCs and it's the same issue for all.

Do you know what could be the problem?

Thanks.