Tool/software:
When open, the corresponding bit in the Remote Channel Open Status Register will be set.
At this time, what is the temperature that can be read in the Remote Temperature register?
Is the following correct?
On short: -256°C fixed temperature
On open: temperature is undefined
■Experimental results
When short: -256°C fixed
When open: -256°C fixed
As my evaluation results,I thought I could read the temperature of -256°C fixed when open.
No remote transistor was connected during the open evaluation.
Cdiff (1000pF) capacitor is connected between D+/D-.
Best Regards,
ttd