Tool/software:
Hi! TI Team!
We currently using the IWR6843ISK and detect the objects like pedestrian and the car.
The overall test showing that the radar can detect the car about 80m when the car is moving forward to the radar.
And for the pedestrian, the distance is about 40m.
But we are curious about the distance that this chip can detect, for the pedestrian is stationary over a point. Like 15m in front of the radar or 25m in front of the radar.
Is there any document or thread can show me how long this IWR6843ISK can detect pedestrian which is stationary?
Best regard,
Webb