This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSS4440: driving ultrasonic sensor over cabling

Part Number: TUSS4440

Tool/software:

Hi team - We are trying to use the TUSS4440 to drive an ultrasonic sensor over a 1m to 3m cable. We did testing on an EVM with the TUSS4440 and ultrasonic on the same board and it worked fine. Now when trying to drive over the cable, the signal at the ultrasonic sensor device is unusable.

Is the TUSS4440 device able to drive the output over any length of cable? Are there any needed design modifications to accommodate driving an ultrasonic sensor over a cable?

Thanks,

Jacob