This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432BOOST: Hardcode which includes two configurations

Part Number: IWRL6432BOOST


Tool/software:

Hello,team

I want to make hardcode which includes two configurations.
These configurations are changed without replacing appimage.
I hope configurations are changed by switch on the board.
Do you have any ideas?

Regards,
Yuichi

  • Hi Yuichi, 

    Sorry for the delayed response. We have an example for switching between two configurations that are both hardcoded into the appimage itself. The example starts in a low power presence detection configuration and then when a person is detected it reconfigures to a higher power tracking configuration. You could use this as a starting point and modify the example to update configuration when the board switch is pressed instead.

    Please refer to the example user guide here and let me know if you have any questions.

    Best Regards,

    Josh