Other Parts Discussed in Thread: AWR2944, AWR1843BOOST
Tool/software:
Hello,
I hope you are well,
Customer is having part which is out of warranty,
Part: DCA1000EVM:
Customer is claiming that :
Part was functional until now and it stopped working. The process of
starting, the sequence of switching on and off the indicator LEDs is not
the same as with a functional unit and it also does not communicate with
the PC in a proper way.
Also the delivered USB A - micro USB cable was in a poor quality and we
had to use a different one.
The sequence in which the LEDs light up and
turn off does not match the sequence on the working board with the same
switch configuration and cable connections. The network is not working and
data is not being transferred to mmWave Studio. However, the board is
noticeably overheating at the location of the largest integrated circuit.
This is not the case with a functioning board.
I do not want to share the picture of the board on public forum.
Could you advise if we can try to make any troubleshooting to help Customer resolve issue if part is defective or not?
Thanks