Other Parts Discussed in Thread: DCA1000EVM, AWR1843AOP
Tool/software:
Hi,
I’m working on synchronizing data captured from a USB camera with raw mmWave radar data acquired from the AWR1843AOP using the DCA1000EVM over Ethernet.
My goal is to achieve synchronization with a maximum timing error of 50 ms. Both the radar and the camera operate at 20 FPS.
Are there any recommended methods or best practices for achieving such synchronization between the radar and camera data streams?
I’ve seen some research articles mention using ROS (Robot Operating System) for synchronized radar and camera data acquisition and visualization. Is there an official or supported TI ROS package that allows capturing synchronized raw radar data from the DCA1000 along with camera input?
Any guidance or suggestions on this would be greatly appreciated.
Best regards,