Tool/software:
Hello Everyone
So we are working on a custom AWR1843 PCB and while we were talking with the manufacturers according to their capability the small traces connecting between two patches of the antenna width is 0.1 mm and they want it to change it to 0.125 mm. So lets say we have made the changes as per the manufacturers so do we also need to change the patch dimension also if we need to change can you suggest us how we can change them having the patch inter connecting line trace width as 0.125 mm to match the 50 Ohm impedance. Also if we just change the patch inter connecting trace width to 0.125mm and do not change the patch dimension what are characteristics changes we will get for the antenna and how we can overcome them. I have uploaded a screenshot of the Patch antenna which is given in the AWR1843BOOST module. You can the small trace which are inter connecting the patches in bellow attached pictures.
Regards
Ratul