This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432AOP: Boot without SerialFlash

Part Number: IWRL6432AOP


Tool/software:

Q1


Regarding the FECSS Firmware Patch, will it be applied even when transferring the user application (via SPI/UART) to run on the M4 core without SerialFlash?
Assuming that the patch binary file, mmwave_rfs_patch_rprc.bin, will be combined with the user application using the tool mentioned in No. 6 and then transferred.

Q2
Is it correct to understand that the following tools included in the SDK are required to create the ImageFile for the user application transferred via SPI/UART?
Please point out any unnecessary tools or additional tools that may be required.${SDK_INSTALL_PATH}/tools/boot/appendBinCrc/appendBinCrc.exe


${SDK_INSTALL_PATH}/tools/boot/crcMulticoreImageGen/crcMulticoreimage.exe
${SDK_INSTALL_PATH}/tools/boot/multicoreImageGen/MulticoreImageGen.exe
${SDK_INSTALL_PATH}/tools/boot/out2rprc/out2rprc.exe

  • Hello

    Q1


    Regarding the FECSS Firmware Patch, will it be applied even when transferring the user application (via SPI/UART) to run on the M4 core without SerialFlash?
    Assuming that the patch binary file, mmwave_rfs_patch_rprc.bin, will be combined with the user application using the tool mentioned in No. 6 and then transferred.

    Please refer to the following thread.

    Q2
    Is it correct to understand that the following tools included in the SDK are required to create the ImageFile for the user application transferred via SPI/UART?
    Please point out any unnecessary tools or additional tools that may be required.${SDK_INSTALL_PATH}/tools/boot/appendBinCrc/appendBinCrc.exe


    ${SDK_INSTALL_PATH}/tools/boot/crcMulticoreImageGen/crcMulticoreimage.exe
    ${SDK_INSTALL_PATH}/tools/boot/multicoreImageGen/MulticoreImageGen.exe
    ${SDK_INSTALL_PATH}/tools/boot/out2rprc/out2rprc.exe

    Please refer to the following thread as it seems to be a duplicate question.

    Sincerely,

    Santosh