Other Parts Discussed in Thread: UNIFLASH, , AWR2944
Tool/software:
Originally, LEDs D13 and D16 were lit, but now only D12 is ON. LEDs D13 and D16 remain OFF. I have not been able to find specific documentation regarding what this status indicates. I believe normally they should all be lit when the device is out of reset. I've tried unplug everything and power cycle it or press reset button, but neither did work. Ever since they do not glow, I cannot use the demo visualizer properly and cannot flash new image (using uart_uniflash_gui.py will result in xmodem error).
-
Board: AWR2944EVM
-
Power Supply: 12V, 3A
-
Software (while it was still working): awr2944_mmw_demoTDM.appimage in SDK ver. 4.7
Any guidance would be greatly appreciated.