My customer is using the TMP275 (High accuracy temp sensor) on some of our products. They’ve looked at the datasheet, and also the one for the TMP75. They can’t see any differences between the parts, is there some way to programmatically differentiate the parts? Is there a bit, or operational behavior difference between the two parts so that they can know in FW which part is installed on the board? Thanks, Bill