This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432AOP: Wakeup source from Sleep/Deep sleep

Part Number: IWRL6432AOP

Tool/software:

Wakeup source from Sleep/Deep sleep

Target radar module can choose a wakeup source among WU_REQIN, SPI_nCS and RTC_CLK_IN.

could you let us know a specification of each signal.

Input signal condition
・WU_REQIN: Logic High/Low change?
・SPI_nCS: General input signal? Only select SPI_nCS for wakeup source?
・RTC: A real clock signal is needed?

  • Hello, 

    Please refer to the power driver example for deep sleep entry/exit (here) which implements wakeup from deep sleep mode from various sources. The example.syscfg file controls which sources are enabled, pin selection, wakeup edge etc...

    Best regards,

    Josh