Tool/software:
Hello, please help to guide the following issues. Thank you
1. The patch itself is fine, there is data transmission, but the initial is not normal (indoor air conditioning room exceeds 98%)
2. At first, I thought there was a problem with the patch, so I used a high- air gun to blow the soldering point, and the re-test showed normal (the initial value was between 60-80%)
3. Later, it was verified the low-temperature air gun was blown (70-80℃), and the re-test result was also OK So I would like to ask you, are any specifications and performance issues that need to be paid attention to for this sensor? In addition, there is still a big difference in the initial value (in the same environment), to ensure that the data is true and accurate?