This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843AOP: Question about Calibration in xWR6843AOP SDK 3.5.4

Part Number: AWR6843AOP
Other Parts Discussed in Thread: IWR6843

Tool/software:

I am currently working with the xWR6843AOP platform, SDK version 3.5.00.04.


I flashed the binary file located at:


C:\ti\mmwave_sdk_03_05_00_04\packages\ti\demo\xwr64xx\mmw\xwr64xxAOP_mmw_demo.bin

For visualization, I used mmWave_Demo_Visualizer 3.5.0 with the configuration file profile_3d_aop.cfg and default value. 


In the Visualizer’s Advanced Command tab, I entered the command:

measureRangeBiasAndRxChanPhase 1 1.0 0.2

However, the system responded with a message indicating that the command is not supported.

I recall that this procedure used to work in the past. Could you please advise if I may have missed a step, or if I am using the wrong file for this SDK version?

Thank you for your support.

Best regards,

Chris.

  • Hi, Chris:

    SDK users guide and Doxygen documentation all indicate that measureRangeBiasAndRxChanPhase should be supported.  Millimeter Wave (mmw) Demo for XWR64XX/XWR68xx/XWR68XXAOP

    Can you add the measureRangeBiasAndRxChanPhase CLI directly to profile_3d_aop.cfg and see whether you will be able to run the visualize successfully.

    Best,
    Zigang

  • Hello,

    I have a question about the recommended calibration process for our IWR6843 boards. Since every board requires individual calibration, I need to know how to properly execute the measureRangeBiasAndRxChanPhase command and write the results using compRangeBiasAndRxChanPhase within the HCC architecture.

    If a direct CLI method is not available in the HCC framework, I am considering the following alternative approach. Could you please validate if this is the correct procedure?

    1. First, load the OOB.bin (Out-of-Box demo) to perform the measureRangeBiasAndRxChanPhase measurement and generate the calibration data.

    2. Then, use a flash API to write this calibration data to a specific, reserved block in the external flash memory.

    3. Finally, flash our mass-production binary, which will be programmed to read the calibration data from that location in flash during initialization.

    Could you please advise on the best practice or the recommended method for implementing this per-device calibration for production?

    Thank you for your guidance.

  • Hi, there:

    Sorry for the delay.  Your proposal looks good to me.  Factory calibration follows a similar procedure.  

    Best,

    Zigang

  • I have a question that I’d like your help with. For the compRangeBiasAndRxChanPhase parameters, is there a recommended flash memory storage address (for example, 0x5008_0000)? Also, which flash API should I use if I want to store the calibration values right after performing calibration?

    Additionally, in the mass production program, where should I modify the storage location of compRangeBiasAndRxChanPhase in flash memory, so that during program loading the calibration values from flash memory can be properly restored into the internal RAM of the IWR6843?

  • Hi, there:

    Please give me some time to find the answer.  Will get back to you early next week.

    Best,

    Zigang

  • Hi, there:

    Sorry for the delay.  In general, you can write to any address offset in the flash.  Just make sure the address doesn't overlap the location in FLASH where application images are stored and has enough space.  Consider an address 0x1ff000 or 0x1fe000 should be a good candidate.

    Best,

    Zigang