AWR2944EVM: AWR2944EVM

Part Number: AWR2944EVM
Other Parts Discussed in Thread: AWR2944

Tool/software:

Dear TI advisor

How can I create the corresponding CCS project based on the awr2944_mmw_demoTDM.appimage provided in the mmwave mcuplus sdk? Could you provide specific steps?

Best regards

  • Hello,

    I would first start with the DDM mss and dss projectspec files present in the radar toolbox at this path

    C:\ti\radar_toolbox_3_20_00_04\source\ti\examples\Out_Of_Box_Demo\src\awr294x

    Using these as a basis you can then use the makefiles in the SDK to edit the files to use the TDM processing chain. One of the main changes is changing the -DMMWDEMO_DDM line to -DMMWDEMO_TDM in the compiler build options section of both projectspec files. You can try this first and import the files and see if they build.

    Best,

    Gabriel