Tool/software:
Hi
Is there a way to flash the appimage over UART (or other means) without having to configure the switches S1.1 and S1.2? We are trying to flash the image as if it were part of an OTA process.
Regards
Tool/software:
Hi
Is there a way to flash the appimage over UART (or other means) without having to configure the switches S1.1 and S1.2? We are trying to flash the image as if it were part of an OTA process.
Regards
Hi, there:
Thank you for reaching us. One of our software engineer will get back to you in a day or two.
Best,
Zigang
Hi Abhishekh,
OTA should be handled by customer Application, UART based Flashing with Switch settings can be used during initial flashing during manufacturing and for further OTA, Application can handle the OTA process.
Regards,
Ajay
My question is how can one flash another appimage without the need to set the switches again.
Hi Abhishek,
Switch settings are required to set the device in flashing mode. Do you mean you want to flash multiple images in one go, when in flashing mode?
Regards,
Ajay