Other Parts Discussed in Thread: MMWAVE-SDK
Tool/software:
Hello,
We are developing a radar using the IWR1843 and are currently building the inspection process for the product.
When we checked the boot-time calibration results (calValidStatus), only the status bit for RX ADC DC Offset calibration showed FAIL.
Please answer the following questions:
Q1: What could be the factors causing the RX ADC DC Offset status bit to become FAIL?
Q2: Is there a required time interval between radar startup and boot-time calibration execution?
Supplementary information:
Among multiple units, only one unit showed FAIL status for RX ADC DC Offset calibration.
The unit that experienced this issue showed the same result on the second boot-time calibration as well.
Both calValidStatus and calValidStatusCpy were 0x80003FDE.
Boot-time calibration is performed 2-3 seconds after software restart.
Best regards,
Yasuaki