IWRL6432: Custom PCB - Won't go into Flashing mode

Part Number: IWRL6432

Tool/software:

I have a custom PCB configured for BOM optimised mode (single 1.8V supply). It's a barebones design with no JTAG adapter on it, so I'm trying to program it using UART with no luck. I don't believe it's going into flashing mode.

SOP0 = 0V

SOP1 = 0V

VDD = 1.2V

VDD_SRAM/VNWA = 1.2V

VDDA_10RF = 0V

VDDA_12RF = 0V

VDDA_18BB/VDDA_18CLK/VDDA_18VCO/VIN_18PM/VIOIN_18 = 1.8V

VIOIN = 1.8V

VPP = Not connected

VBGAP = 0.9V

VOUT_14APLL = 0V

VOUT_14SYNTH = 0V

Clock is oscillating at 40 MHz.

I believe in flashing mode the clock should be disabled, and it VBGAP shouldn't sit steadily at 0.9V? 

Do you have any advice?