Other Parts Discussed in Thread: LDCCOILEVM, FDC1004
Tool/software:
My name is Yash, and I am a graduate student working on liquid conductivity measurements. I am currently using the LDC1612EVM evaluation board, which comes with coils connected to each of the two channels. To experiment with different inductance values and Q-factors, I also purchased the LDCCOILEVM evaluation board for testing alternative coil configurations relevant to my application.
In my experimental setup, I poured a salt solution into a glass container and situated the coil on the outer wall of the container. The coil was connected to the evaluation board, which was then connected with my computer and I tracked my measurements via the TI GUI for inductive/capacitive sensing. Now, when I increased the conductivity of the solution inside the container, the GUI consistently showed that the inductance of the coil increased as well.
I would like clarification on the following points:
-
Cause: What possible physical mechanism causes the inductance to increase with increasing solution conductivity?
-
Correctness: Is this response expected, or could it be an artifact / error of the measurement system?
-
Application: Can this method serve as a reliable, non-invasive, contactless approach for liquid conductivity measurements?
Note: For experimental consistency, I ensured that the liquid volume inside the container remains constant across all conductivity levels.
Thank you for your time and guidance.
Best regards,
Yash