AWRL6844EVM: Example code request for AWRL6844EVM (mid-level MSS+DSS project with DSP and HWA)

Part Number: AWRL6844EVM
Other Parts Discussed in Thread: AWRL6844

Tool/software:

Hi team,

I am working with the AWRL6844EVM board. Currently, I have two example projects:

  • mmWave Demo from MMWAVE_L_SDK_06_00_05_01\examples\mmw_demo (runs on MSS only with HWA, relatively simple).

  • In-Cabin Demos from radar_toolbox_3_20_00_04 → Automotive_InCabin_Security_and_Safety\AWRL6844_InCabin_Demos (runs on both MSS and DSS, uses HWA and DSP, and supports CPD/SBR/Intruder detection – much more advanced).

I am looking for something in between these two. Specifically, an example that:

  • runs on both MSS and DSS,

  • includes processing on both DSP and HWA,

  • but is simpler than the In-Cabin Demo (i.e., without the full CPD/SBR/Intruder application pipeline).

Is there any mid-level example project available for the AWRL6844EVM that demonstrates this kind of setup?

If not, could you please provide some guidance or documentation on how to extend the mmWave Demo into an MSS+DSS project with both DSP and HWA processing, step by step?

Thanks in advance

Best regards,
Beyzanur Cam

  • Hi, there:

    Unfortunetely, we do not have anything in between.  The two demos are actually developed parallely.  The in-cabin demo is not developed after SDK OOB demo.  Therefore, we do not have any step-by-step guide to change from one to the other. 

    We have in-cabin users guide.  You can find the block diagram inside.  That can give you some idea how the communication between DSP and ARM core is done.  

    Best,

    Zigang