Tool/software:
Dear TI Team,
I have a question regarding antenna calibration for the AWRL6844. Our team is using the 6844-related application in radar_toolbox_3_20_00_04.
In the range_phase_bias_measurement.c
file, why is the collected data multiplied by the bpmsign
value (as shown in Figure 1)? All configurations—including ID, CPD, and SBD—are using TDMA mode.
Additionally, could you confirm whether the loop in Figure 1 is incorrect? Based on the current implementation, it seems that the index does not change according to the Tx antenna index.(From RadarCube)
Lastly, why does the calibration is not allowed when clutter removal is enabled? The data used is from RadarCube—could this be affecting the results?
Figure(1)
Sorry, I have some questions I'd like to ask.
In dynamicCfarConfig setting:
Is the product of the azimuth size and elevation size being used as the fft2DSize
?
If so, could this cause discontinuities in the signal and potentially affect detection performance?
Thank you for your assistance.
Henry Lin