Other Parts Discussed in Thread: TMAG5273,
Tool/software:
Hello support team,
We are considering of using TMAG5173A2 (or TMAG5273) to monitor magnetic field generated by a magnet for a time period of few years. The absolute accuracy is not as crucial as stability/repeatability of measurement.
We would like to learn more about the sensitivity specifications shown in datasheet.
A sensitivity error specification at certain temperature gives a maximum error of 3.3%. Is this sensitivity error something that remains more or less constant through the lifetime of the component or does this sensitivity error change through the years? For example, if the error of a sensor in the beginning is 2%, is it ok to assume that after 2 or 5 years this error is still 2% in this sensor, if temperature is kept constant?
Another spec is Sensitivity lifetime drift with max. value of 4.9%. This drift spec clearly suggests that sensitivity will change in time. But what is this "lifetime"? Is there a way to estimate this drift for example after 2 or 5 years? Is it a linear function of time? Also, is this lifetime sensitivity drift something that needs to be added to sensitivity error, so that the overall maximum drift could be in the order of 3.3% + 4.9 % after some period of time? Or how could we estimate the total drift of sensitivity as a function of time?
Texas also has a model TMAG5273A2. For this model the datasheet does not specify sensitivity lifetime drift. Is it ok to assume that lifetime drift for TMAG5273 is somewhat similar to TMAG5173, since these models seem to be some sort of "siblings" in many ways?
Best Regards,
Marko