AWR2243BOOST: AWR2243Boost Continue Real-time Radar measurements

Part Number: AWR2243BOOST
Other Parts Discussed in Thread: DCA1000EVM, AWR2243, AWR2944, AWR1843

Tool/software:

Hi 

As i am using AWR2243Boost with DCA1000EVM , but the output by DCA1000EVM is good but its not realtime , discreate, and the same set up we can not use for our application, So what target board /Embedded Processor eval kit we can use to configure AWR2243Boost for realtime continue output ,

1. My concern is to replace DCA1000EVM with some Embedded Processor that can program/configure AWR2243 and in Embedded processor we can implement DSP applications , please provide some suitable solution with AWR2243Boost + target platform/bare metal/embedded processor(which embedded device such as can be supported with TI provided DFP or visual studio setuo for NonOS platforms)

2. If we use  AWR1843 or  AWR2944 EVM (Radar Soc so we can configure AWR2243Boost as it has its own processor ) but in that case also DCA1000EVM is needed to capture the data  and again DCA1000EVM is not giving continue real time output . so which platform /target board we can use for AWR2243Boost or  AWR1843 and AWR2944.

Please suggest 

thankful fot your valuable inputs

Hemanth_ast