Other Parts Discussed in Thread: DRV411
Tool/software:
Dear TI experts,
Now my customer check the specification of DRV401 for their new project.
In the datasheet they found that DRV401 needs "field probe" because DRV401 itself is signal conditioning IC, not sensor.
And here are my questions ;
1. Should I use only "Field probe" component with DRV401? Or is it okay to use other components like hall element IC or TMR(tunnelling magnetoresistance)?
2. If the answer about no.1 is yes, should I use only the component of VAC(VACUUMSCHMELZE) which is mentioned in the first page of datasheet? Or Is it okay to use other companies?
Could you suggest the vendor of "Field Probe" exclude VAC?
3. Is there any patent for the "Field Probe" or any other added components which are used with DRV401? I saw about "Patent Pending" in the diagram in the first page of datasheet.
My customer is worried about the patent so they cannot use any component what they want freely.
Please chech these issues. Thanks.
Best regards,
Chase