Tool/software:
Hi expert,
When using TMP75 in standard mode I2C, customers tested that the SDA_rise time is 731.5ns/SCL_rise time is 771ns/SDA_hold time is 2.687us. All these 3 are beyond the range listed in timing requirements of fast mode in the datasheet. While these parameters fulfill the standard mode requirement in I2C standard. So my customers would like to confirm if these parameters are ok under I2C standard mode when using TMP75?
BR,
Manu