Tool/software:
We designed a people presence, and vital monitoring device using the IWR6843ARQGALPR mmWave Radar. The radar is powered by a PMIC LP87524JRNFRQ1 and voltage regulator TPS62130ARGTR.
During the EMI scan, we experience a high emission at 400Mhz from the antenna and PMIC. We aren't able to isolate the noise as both ICs are next to each other.
These are my questions:
1. According to TI's reference design, the input voltage to the PMIC is 3.3V. If the voltage is greater then 4V, a snubber components are needed at the output nodes to reduce EMI. Is there any reason we have to drive the PMIC at 5V?
2. TI recommended X7R type capacitors for both input and out. What is we go wIth X5R capacitors?
3. We power the PMIC using 5V, but without snubbers installed. Does this cause the 400MHz emission?
Best Regards,
Bryan