Tool/software:
Could you please confirm that all pins named Tsense are electrically connected internally? Do we have any test data indicating the impact on temperature reading if one of the Tsense pins isn't connected?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Could you please confirm that all pins named Tsense are electrically connected internally? Do we have any test data indicating the impact on temperature reading if one of the Tsense pins isn't connected?
Thank you!
Lenio,
The TSENSE pins are all connected to each other in a single piece of leadframe, but they have no electrical connection to the die. The TSENSE pins just serve as thermal connection pins, to allow heat transfer to the die through the isolation barrier.
If the user only connects one or some of the TSENSE pins, the only outcome would be that the temperature response would be slowed to some degree. The unconnected pins would only pick up heat through radiation not direct conduction through the copper. But the core functionality of the device would not be impacted, just the performance.
Thanks
-Alex Thompson