Other Parts Discussed in Thread: DCA1000EVM, MMWAVE-SDK
Tool/software:
Hi,
Currently I have acquired an AWRL6844EVM + DCA1000EVM modules to generate and read radar data directly as raw ADC data onto my laptop. The idea behind this is to obtain through our application the heatmaps or Range-Doppler, Range-Azimuth and Range-Elevation. My problem is related to a specific question.
When I apply 2D Capon algorithm to obtain the angles using the beamforming, I'm using a system in which the boresight is the +Y axis and the virtual array antennas follows an UPA array according to documentation:
dev.ti.com/.../node
Before applying Capon, I was apply FFT over slow and fast data and a TDM compensation and static cluttering removal process, but the system will always locate the targets to 0º. I think that this could be related to the calibration because I was not applying any kind of system calibration or vector calibration in my application.
Currently, I'm using mmWaveStudio 4.3.1.0 for configuring the completely system and the mmWave-sdk_6_0_5_1 for obtaining the feccs and other files required by the radar, but the problems refers that I've never applied a calibration neither the factory or another and I do not know where I can obtain the factory calibration values to use it in my application to avoid the 0º positioning of my targets.
Could you help me with this topic or provide me a way to proceed to obtain that vector calibration values?
Greetings,
Sergio.