This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: Zero Insertion VS shuffleLUT

Part Number: AWR2944


Tool/software:

Hi,

Can "zero insertion" be configured like shuffleLUT, where multiple zero inserts can be set at once, but when used, the offset is used to control where to start, 
as shown in the below

    shuffleRamOffsetAzimFFT = 16*2*sizeof(uint16_t);
    retVal = HWA_configRam(obj->hwaHandle, HWA_RAM_TYPE_SHUFFLE_RAM, (uint8_t *)&cfg->staticCfg.azimFFTGeometryCfg[0], \
                                                sizeof(uint16_t)*NUM_TXANT*NUM_RXANT, shuffleRamOffsetAzimFFT);

    shuffleRamOffsetElevFFT = 16*3*sizeof(uint16_t);
    retVal = HWA_configRam(obj->hwaHandle, HWA_RAM_TYPE_SHUFFLE_RAM, (uint8_t *)&cfg->staticCfg.elevFFTGeometryCfg[0], \
                                                sizeof(uint16_t)*NUM_TXANT*NUM_RXANT, shuffleRamOffsetElevFFT);
                                                
    // use
    hwaParamCfg.source.shuffleStart   = 2;
    hwaParamCfg.source.shuffleStart   = 3;

Thanks!