Hi team,
The customer found in previous projects when using XA2944BD that after importing HSM, they needed to increase clockP_sleep(1000U) to 4000U for the code to run normally, otherwise there would be a 5-second delay stuck between load HSM and SBL.
Currently, when the customer uses AWR2944BS, after importing HSM and setting clockP_sleep to 4000U, there is still a probability of experiencing a 5-second delay stuck before SBL. And current remains at 139mA. Has the team encountered this issue internally? The SDK and chip versions are as follows:
SDK version is 4.6.1.02 + 09.02.15, and the AWR2944 model is shown in the figure.