AWRL1432: AWRL1432 software debug

Part Number: AWRL1432
Other Parts Discussed in Thread: MMWAVE-L-SDK

Dear Engineer,

We are using AWRL1432, and the official information provided includes <awrl1432_entry_level_blind_spot_detection> , but there is no source file, only a burned file. We want the source file so that we can quickly develop the product. Can it be provided?
In addition, there is also the <awrl1432_adas_bsd_demo v 2.1> file. Can it be provided?
If there are other AWRL1432 related materials available for familiarizing oneself with the chip and internal functions, can they be provided?
Thank you!

  • Hello,

    Thank you for reaching out. We cannot share the source code for the AWRL1432 BSD Demo, but for more development resources, please view the following:

    Please let us know if there are any other resources we can provide here.

    Cheers,

    Kristien