AWR2944P: AWR2E44ECO: There is no TX3 in rlAllTxPowMonConf structure

Part Number: AWR2944P


Hi,

I downloaded latest DFP for AWR2x44P series, but there is no TX3 in rlAllTxPowMonConf stucture. Would you pls kindly advise if the firmware can't monitor TX3 power or it is missed in the header file?

mmwave_dfp_02_04_18_01\ti\control\mmwavelink\include\rl_monitoring.h

typedef struct rlAllTxPowMonConf
{
    /**
     * @brief  Power Monitoring Configuration for Tx0
     */
    rlTxPowMonConf_t *tx0PowrMonCfg;
    /**
     * @brief  Power Monitoring Configuration for Tx1
     */
    rlTxPowMonConf_t *tx1PowrMonCfg;
    /**
     * @brief  Power Monitoring Configuration for Tx2
     */
    rlTxPowMonConf_t *tx2PowrMonCfg;
}rlAllTxPowMonConf_t;
 
Thanks,
Chris
  • Hello Chris,

    That was for the older devices and if someone was using 3 Txs they can continue with that Structure..

    There is a function: rlRfTxnPowrMonConfig where we can configure all the 4 Txs. The previous one was kept only for ease of porting.

    Regards,
    Saswat Kumar