AWR6843AOPEVM: Inquiry about AWR6843AOP-EVM suitability for static 3D environment mapping

Part Number: AWR6843AOPEVM
Other Parts Discussed in Thread: AWR6843AOP, IWR6843AOP, AWR2944, AWRL6844

Dear TI Support Team,

Hello, our team is currently using the AWR6843AOP-EVM to collect 3D position data of surrounding static objects (e.g., obstacles, walls, ceiling, floor). However, we noticed that most of the SDK example demos are optimized for dynamic object detection and tracking.

 

We attached our short video showing a person walking. The green points represent detected human movements, which appear to be captured faintly. However, the red points are mostly classified as noise. Below are the parameters we used for the experiment.

6843AOP_Standard2.cfg 

We would like to ask a few questions:

  1. Is this radar sensor (AWR6843AOP-EVM) suitable for capturing static environment structures in 3D, or should we consider using a different sensor? we used radar in  2~ 10 meters

  2. Since radar point clouds are relatively sparse, it is often difficult to determine whether a point is reliable or just noise. Would it be feasible to fuse radar data with a depth camera to verify and filter out unreliable points? 

  3. Are there any recommended methods or algorithms to distinguish noise from valid static points when using the AWR6843AOP-EVM?

Thank you very much for your time and support. We look forward to your advice.