AWR2944EVM: Can't use web demo visualizer to show detection result.

Part Number: AWR2944EVM
Other Parts Discussed in Thread: AWR2944,

Hello Experts,

I flash "out_of_box_2944.appimage" in radar_toolbox_2_30_00_12\source\ti\examples\Out_Of_Box_Demo\prebuilt_binaries and use web demo visualizer to show detection result. But the visualizer show this error message "SDK input version [major,minor]=[0,8] not matching [4,4] reported by target." Can you please help to check the reason?

Radar board: AWR2944 Evaluation Module

radar toolbox version: v2_30_00_12

example: source\ti\examples\Out_Of_Box_Demo\src\awr294x

web demo visualizer: dev.ti.com/.../

I already change the SDK version in setup details which is ver4.4 same as firmware version that i flash in AWR2944EVM but still got this error. why?

Regards,

Bayhaqi Mohd Jailani

  • Hello,

    Please acquire the app image from the newest SDK (download available on TI.com). Here is the path to the relevant app images

    C:\ti\mmwave_mcuplus_sdk_04_07_01_04\mmwave_mcuplus_sdk_04_07_01_04\ti\demo\awr294x\mmw

    You are using what seems to be an old demo.

    Also verify you are using the newest visualizer version as well.

    Best,

    Gabriel