Part Number: TMP421
Hi team,
We are considering using the TMP421 to measure the temperature of our device. The device has TEMP_A (anode) and TEMP_K (cathode) pins for temperature measurement, with an internal diode embedded between them. We plan to apply approximately 4.0 V to TEMP_A and 3.3 V to TEMP_K, assuming that the forward voltage (Vf) between TEMP_A and TEMP_K will vary depending on temperature. We expect the voltage difference to be in the range of 0.67 V to 0.78 V.
Questions:
-
We are considering using the device in the manner described above. Is this usage appropriate?
-
Since the register resolution is 0.0625 °C/LSB (1/16 °C), does this mean that the internal ADC resolution is approximately 12 bits?
Best regards,
Kyohei