Part Number: IWR1843BOOST
Other Parts Discussed in Thread: DCA1000EVM, , UNIFLASH
I am currently using the IWR1843BOOST together with the DCA1000EVM, and I would like to request technical support regarding an issue that started after flashing the board.
- Hardware: IWR1843BOOST + DCA1000EVM
- mmWave Studio: 02_01_01_00
- UniFlash: 8.2.0
- CCS: 8.3.1
- mmWave SDK: 3.6
Issue Description
Until yesterday, I was able to use MATLAB and the mmWave Demo Visualizer without any special flash configuration. However, after I used UniFlash to upload/flash the image file ccsv8_xWR18xx.bin, both MATLAB and the mmWave Demo Visualizer have stopped detecting/loading the DATA PORT(COM4).
I tried multiple troubleshooting steps such as reconnecting the hardware, power cycling, and rebooting Windows, but the issue persists.

In addition, when attempting to connect via mmWave Studio after this happened, the BSS FW version is detected as 0.0.0.0, and mmWave Studio becomes unresponsive while trying to download the MSS (the program appears to freeze).


Support Requested
Could you please help with the following items?
2. Recommended troubleshooting steps or root-cause guidance for resolving the DATA PORT not being recognized after flashing.
Thank you very much for your time and support.