Part Number: AWRL6432BOOST
Other Parts Discussed in Thread: UNIFLASH, IWRL6432
Auto detected



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can you please check if you have configured the SOP switches correctly in flashing mode. Also please ensure that you have selected the correct COM port. You can get more details in the AWRL6432BOOST EVM user guide.
https://www.ti.com/lit/pdf/SWRU596
Regards,
Sreedeep
Yes, I made Switches accordingly for flashing Mode. and COM port selected as Auto mode.
Hi,
Can you show a snap of the device manager COM ports. Are you seeing XDS com ports in it. Also is the board powering up when you are connecting the USB.
Regards,
Sreedeep
Hi Sreedeep,
See Here COM Ports 13 as Application User Port as below image

then operated Sensor in functional mode then Vital Signs not appears as shown below image

So now i want to flash Vital Signs so i changed SOP mode in Sensor Switches positions as shown below image

Launched Uni Flash
And used Auto Detect Option and Clicked on Start

Then Selected image file


it says please power cycle; i need to something here or just load?
i just clicked on load image

what to do now?
Hi,
I can still see that the error is serial COM1 specified doesnt exist. That means it's still taking the default COM port in Uniflash. Your XDS COM port is 13 as I can see from device manager. You have to manually type in the COM port by going to settings and utilities tab. Please try that and let me know.

Regards,
Sreedeep
After Changing Com13 in Manual Settings, i can able to flash and Operated Successfully.


I can't See the Sensor Frequency Range for Vital Signs, but I measured manually and confirmed that it was 60-61.6GHz.
Now i have few Questions regarding Vital Signs Windows.
1. What is the Accuracy of Heart Rate and Breath rate?
2.Max and Min Range detectable by Sensor?
is there any info Regarding Vital Signs windows , Please Share.
Thank you for Solving to Successful connection with Vital Signs.
HI, there:
Are you using IWRL6432 vital sign demo listed below? radar_toolbox_folder\source\ti\examples\Industrial_and_Personal_Electronics\Vital_Signs\IWRL6432_Vital_Signs
Could you start a new e2e and mentioned the IWRL432? It is supported by a different group.
Best,
Zigang