This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP1075: Exposed pad connection of TMP1075DSG package

Part Number: TMP1075

Hi,

I'm thinking if using TMP1075DSG (2mmx 2mm) package in my design and I have a question regaring its exposed pad conenction. 

In my design, TMP1075DSG is used to sense the temperature of a copper plane which is covered with solder mask and the copper plane is not at ground potenetial. The copper plane with solder mask will be between 0.5V to 2.5V. 

The datsheet of TMP1075 shows exposed pad conenction to ground plane and ground plane is mentioned as "heat source". This is different from my application where heat source is not ground. 

May I know your recommendation on how to connect TMP1075DSG exposed pad in my application? Can I leave it floating or does it need to be grounded? If I leave it floating, would it still sense the underneath copper plane temperature eventhough the copper plane has solder mask?