This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3004: Inquiry regarding ambient light sensor recommendation

Guru 12655 points

Part Number: OPT3004

Hello,

My customer is looking for an ambient light sensor solution for indoor and outdoor light measurement, battery operaion.

Please recommend a TI product that meets the following requirements:

  - Operating voltage : 1.7-3.4V(for use with 1.8V, 3.0V and 3.3V)

  - Current consumption : Lower is better

  - Communication I/F : I2C

  - Light range and resolution : 

        High sensitivity and accuracy are not required.

        Used to determine whether lighting is needed indoors (outdoors).

Thank you.