Part Number: TMP103
Hi experts,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMP103
Hi experts,
Hi Harry,
We need the RX specification for the thermal sensor at 1 MHz. Please confirm whether the data below meets your requirements.
| Symbol | Parameter | Test Result | Unit | |
| Min | Max | |||
| fSCL | SCL clock frequency | 0.909 | 0.914 | MHz |
| tHD;STA | hold time START/RESTART condition | 348.786 | 348.786 | ns |
| tLOW | LOW period of the SCL clock | 550.677 | 555.646 | ns |
| tHIGH | HIGH period of the SCL clock | 520.124 | 522.732 | ns |
| tHD;DAT | data hold time | 97.301 | 103.442 | ns |
| tSU;DAT | data set-up time | 424.913 | 454.397 | ns |
| tSU;STO | set-up time for STOP condition | 5815.833 | 5815.833 | ns |
| tSU;STA | set-up time for a repeated START condition | 5809.646 | 5809.646 | ns |
| tr-SCL | rise time of SCL signals | 17.829 | 23.614 | ns |
| tr-SDA | rise time of SDA signals | 23.044 | 23.044 | ns |
| tf-SCL | fall time of SCL signals | 1.294 | 1.388 | ns |
| tf-SDA | fall time of SDA signals | 1.687 | 1.733 | ns |
| tVD;DAT | data valid time | 99.029 | 126.487 | ns |
| tVD;ACK | data valid acknowledge time | 244.18 | 244.18 | ns |
Hello YI YUN LIN,
From my observation, I don't see anything concerning with the data collected. The most important parameters that must be adhered to are the data hold time (HDDAT) and data setup time (SUDAT) and the values observed in your setup comply with what's provided in the datasheet. 
Regards,
Harry