Part Number: AWR6843AOPEVM
Below is output from Area Scanner for the mmwave radar 6843AOPEVM.pdf
Please read the attached since it shows and explains the issue I'm having when parsing the data. There are 4 extra bytes of 0s that are not added to meet a 32 byte boundary and should not be there from all the TI docs I read. Someone has to be used to looking at the binary output to understand what I'm saying. Please help! From what I know today the TI AreaScanner firmware is sending out extra 0s that should no be there and because they should not it messes up my parsing of the frame header to the first type identifier, which in this case is Type 1 for the 6843AOPEVM. This is time sensitive.