Part Number: TMP117
Hi,
Our TMP117 sensors are embedded in a finished product, so we can't physically inspect the package marking. We'd like to verify them via the factory-programmed Unique ID (EEPROM1/2/3).
Readings:
Device 0x48: EEPROM1=0x4F6D EEPROM2=0x0F82 EEPROM3=0x0E04 -> assumed ID: 0x4F6D0F820E04
Device 0x49: EEPROM1=0x4F89 EEPROM2=0x0F69 EEPROM3=0x03D8 -> assumed ID: 0x4F890F6903D8
Questions:
- Can you confirm the correct byte order for constructing the 48-bit Unique ID from these three registers?
- Do these IDs match valid TI production records, and if so, which variant (TMP117/M/N) and package?
- How do we request NIST/ISO 17025 calibration traceability documentation for these serials -- via Unique ID alone, or do we also need lot/date code from the part marking?
- Is there a self-service tool for this, or is a manual request required each time?
This is for supplier part verification on a finished product where the chip isn't visually accessible.
Best Regards,
Kittitouch Lelapiyamit