Part Number: AWR2243
I am cascading 4 TI AWR2243 chips. Out of 4 chips, 2 work as TX only with external LO_syn and other 2 as a RX only Chip with Ext LO_syn. There is one more Awr2243 chip Which is used as master for LO_Syn, Clock and trigger and there will be no Active TX or RX channel for it. The 2 TX only chips works in transmit mode and no receive channel works there. The TX only chips transmit Sequentially with only one TX antenna(channel) active for a Chirp. The 2 RX only chip will work in receive only mode and receive simulataneously for RX channel but none of its transmit channel active. I need to know how much current(average and peak) and voltage required for each type of chip per rail. How much DC power consumption for each chip: Tx only; Rx only chip and master chip with no active tx and rx channel