LDC5072-Q1-SENSOR-DESIGN-TOOL: LDC5072 Sensor designer hangs

Part Number: LDC5072-Q1-SENSOR-DESIGN-TOOL

I'm trying to use the designer for a sensor with an 8:1 electrical to mechanical ratio, but it hangs every time the "Compute Spice Model" gets to the bit where it tries to fit a curve to Target-Sense inductance data. Exact same geometry works for any electrical to mechanical ratio less than  8:1. No amount of fiddling with the geometry seems to work at 8:1 or higher.

Is this a fundamental limitation of the simulation tool?

Example of the failing setup :  SensorDesign1.zip 

Side note: I have quite a bit of freedom with respect to the inner and outer diameters of the sensor. Is there an optimum ratio for best accuracy?