Dear All,
Please clarify me about the configuration issues related with TMP102. We have initialized the TMP102 device CONFIGURATION register as follows... byte1: 0x62 byte2: 0xA0. (At that time the default values in the other registers are: Reg0: 0x30 0x90, Reg2: 0x4B 0x00, Reg3: 0x50 0x00 )
Once we change the Temperature threshold values (TLOW and THIGH) dynamically by an application to 25 and 30 degrees , we got the first interrupt. But after this the CONFIGURATION register value has changed to byte1: 0x60 byte2: 0x40. Interesting thing from this is, once you set the threshold value, CR1 and CR0 bits value got changed and also the TM bit has changed from 1 to 0.
Is this an expected behavior in TMP102 device ?
Regards,
Hareesh