I have designed my NTC Thermistor circuit based on reference sloa052 and sboa097.
But the input temperature range is from -40C to +150C instead of from 0C to +100C.
When input temperature is -40C, the resistance of Thermistor is 191908 ohm, which means the input voltage will be +20V if I use REF200.
I have selected Circuit 2: Single-Supply/Single-Part Approach in sboa097 to reduce the input voltage down to +3.3V ADC interface.
Please send me any suggestions if my idea is practical.
Many thanks.