This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How can reset LM73

Other Parts Discussed in Thread: LM73

All

Do you know how can reset LM73?

  • Hi Seasat,

    The only way to reset the device is power down.

    Aaron Heng

  • Hi Seasat,

    I may not be clear regard to the implication of power down. Yes, you can reset the device. It can be power cycling the part or a software power down. Here are the step sequences for software power down. For more detail, please refer to the LM73 datasheet section 3.3.

    1. Allow Vdd reach to the minimum operating voltage (+2.7V) as specified in the datasheet in the Operating Rating section.
    2. Write a “1” to the Full Power Down bit 7 of the configuration register. Hold it high for the specified maximum conversion time for the initial default of 11-bit resolution, which is 14ms.
    3. Write a “0” to the Full Power Down bit to restore the LM73 to a normal mode.

    Aaron