Other Parts Discussed in Thread: TMP006
Hello,
I am having trouble getting the correct value of object temperature tobj using the fixed point code . The value of Tdie is absolutely correct so the sensor TMP006 is working absolutely fine. However the output of the Fixed point calculation code is incorrect . It gives the value of Tobj such that it provides a value (on the LCD) in the range of 32 to 36 degree Celsius no matter what i place in front of it.