We've read many of the posts here related to the TMP006, and downloaded useful calibration spreadsheets and sample code.
In our application the TMP006's field of view will be the underside of a heatsink we wish to monitor. An accuracy of +/-3 C is acceptable over Tdie and heatsink range of -20C to +70C. In our application, Tdie and heatsink temp are not related and don't trend together. We can gather two calibration points with a constant Tdie to obtain our calibration constant - at the lowest and highest expected heatsink temperatures. We intend to use the 'transient temp correction' discussed in this forum.
My questions are:
1) Is the calibration data taken at Tdie=20C still valid for calculating the remote temp in actual use when Tdie varies between -20C and +50C?
2) Is the calculated remote temp accurate if the remote temp is significantly colder (say -10C) than Tdie, and Tdie is significantly higher than when the cal data was taken (say Tdie=50C)?
3) Can the cal data be gathered at elevated Tdie (say 50C) if we can hold Tdie constant? (remote temp would be -20C to +70C)
Thanks,
Jim D.